About the Approval Cockpit Application
You can use Approval Cockpit to create and execute approval workflows for action events raised in Plant Applications.
For example, to release a route in the Route Editor application, the event must pass through an approval workflow process in the Approval Cockpit application. The delegated approver groups in the workflow must provide their approval before releasing a route. Similarly, to dispose a defect in the Non Conformance application the delegated approver groups in the workflow must provide their approval in the Approval Cockpit application.
After you configure an approval workflow for an action event, the execution of the workflow becomes an automated process whenever the respective event is initiated in Plant Applications. The delegated groups log in to the Approval Cockpit application to access the tasks awaiting their response, and can track the status of the workflows in progress.
mes.approval_cockpit.user
scope.As an administrator, you must complete the following tasks to enable the workflow configuration and execution in Approval Cockpit:
- In Plant Applications Administrator,
- Verify that the action events for Approval Cockpit are available as production units under Plant Model > APC Department > APC Line.
- Verify that each production unit also has a variable group to list variables related to the action events.
- In Approval Cockpit,
- In Plant Applications Administrator, for every workflow configuration:
- Verify that the display sheets are available under Client Management > Displays > APC Line. Create display sheets with the naming convention: ProductionUnitName_WorkflowLevel_WorkflowGroup. Tip: Display sheets for a typical two-level workflow can look like this:
Route Approval Form_Level 1_Approvers 1
Route Approval Form_Level 1_Approvers 2
Route Approval Form_Level 1_Monitoring
Route Approval Form_Level 2_Approvers 1
Route Approval Form_Level 2_Rejection
- Verify that the variables are linked to the display sheets. Modify the display sheets to set display options and variables.
- Verify that the display sheets are available under Client Management > Displays > APC Line. Create display sheets with the naming convention: ProductionUnitName_WorkflowLevel_WorkflowGroup.
- In Approval Cockpit, as a supervisor, you can: