About OEE Aggregation Store
The OEE Aggregation Store is designed to improve the performance of the following screens on Plant Applications Web Client:
- OEE dashboards
- Reports
- Downtime KPI
- Waste KPI
The values are populated within the OEE Aggregation Store database table. The OEE Aggregation Store is managed by the following parameters:
Value | Result |
---|---|
True | Enables the population of the OEE Aggregation tables and use of the tables on the screens. |
False | Disables the population of the OEE Aggregation tables and use of the tables on the screens. |
Value | Result |
---|---|
1-24 | Defines the number of hours worth of data to refresh. For example: The OEE Refresh Intervals value is set to 5. At 2 PM the OEE Aggregation store table is updated to show values for 2 PM, 1 PM, 12 PM, 11 AM, and 10 AM. |
Note: The OEE Aggregation Store functionality will not be leveraged in existing Plant Applications
Client.