About My Machines
As an Operator, you can use the My Machines application to select machines from the list of machines accessible to you across a plant model. The selected machines are set as your user preferences in the Plant Applications Web Client. The other applications in the Plant Applications Web Client, such as Downtime and Reports, display their application-specific data for only those machines that were set as your user preferences.
Note: Two user preferences are stored for a user. You can switch back to previous user preference using the Restore Previous Profile option.
My Machines provides two types of views: Exclusive and Inclusive. When you access the application, you can see these two views in respective tabs.
- Exclusive: Allows you to select machines from the list of machines accessible to you across a plant model.
- Inclusive: Allows you to create your own profile and add machines to it.
When you load the My Machines application for the first time or if no machines are displayed, the machines for which you have access to appear in the Selected Machines section.
Note: If no machines are authorized to you, an error message is displayed. Contact your System Administrator.