Add a Reason Comment to an Alarm
About this task
Use this procedure to add a Reason comment to an alarm using the following:
- The Initial grid
- The Comments icon
Procedure
- In the Initial grid, select the Edit icon (
).
The Edit page appears.
Select the Reasons tab, and then select Add/Edit Comment.
An editor to add a comment appears.
Enter your comment, and then select Add.
- To add a Reason comment using the Comments icon
(
), select the icon under the Comments column.
The Comments page appears.
Select the Reasons tab, and then select Add New Comment.
An editor to add a comment appears.
Add the required comment, and then select Add.
The alarm is updated with a Reason comment.