Create a Workflow
This topic describes how to create a basic workflow for approvals.
Before you begin
About this task
Procedure
- In the Approval Cockpit page, on the Approver Configuration tab, select
.
The Add Workflow Details screen appears. - Provide values as specified in the following table.
Field Description WORKFLOW NAME Enter a unique name for the workflow that does not exceed 100 characters. SELECT FORM Select a form to use with the workflow. This box contains a list of forms defined for the Approval Cockpit workflows. These forms are production units created under the Approval Cockpit department and line in Plant Applications Administrator. A set of variables associated to the form or unit serve as an approval questionnaire. PRODUCTION LINE Select a production line to which the workflow belongs. This box contains all the production lines defined in Plant Applications Administrator. - Select Add.The Create New Workflow page appears with the added workflow details.
- Add the first level of approvers in a workflow.To create and save a basic workflow, you must add groups under the Approvers 1 section.
- Select Save.The workflow is saved to the list of workflows on the Approver Configuration tab.
What to do next
- Add a monitoring group, rejection responding group, or escalation responding group.
- Add another level to your workflow.
- In Plant Applications Administrator, ensure that the display sheets are created for the configured workflow under the client management section.