Add Approvers Group
The groups listed under the Approvers 1 section, under Level 1 are the initial approvers in a workflow.
Before you begin
About this task
Procedure
- In the Create New Workflow page, under the Approvers 1 section, select Add.The Add Alternative Approver Groups screen appears with a list of group names.
- Select the check box for the groups you want to assign as approvers to the workflow.
- Select Add.The selected groups are listed under the Approvers 1 section. The workflow process requires any one group among the selected groups to provide their approval.
- To add additional approver sections in the same level, select Add New Approver Group, and repeat steps 2 and 3 to add approvers.Every additional section in the same level is incrementally labeled. For example, Approvers 2, Approvers 3, etc. The sections are added with an AND operator implying that the approval workflow must pass through all the approver sections in the given order.
- Select Save.The workflow configuration is saved.