Add a Workflow Level
Workflows can have one or many levels of approval processes. By default, every workflow has one level labeled as Level 1.
Before you begin
About this task
Procedure
- In the Create New Workflow page, select Add New Level.A new level is added to the workflow. New levels are labeled incrementally, such as Level 2, Level 3, etc.
- To insert a level above an existing level, select
on any existing level, and then select Add new level above.
A new level is inserted above the existing level. - To insert a level below an existing level, select
on any existing level, and then select Add new level below.
A new level is inserted below the existing level. - Select Save.The workflow configuration is saved.