|
Label |
The text that appears for components such as check boxes and
drop-down list boxes. |
Global Data |
Allows the data to be available globally for use by other
components or query inputs. This check box is enabled only after
you specify an Id for the
component. |
Allow Export |
Indicates whether data that appears in the component can be
exported. By default, this check box is cleared. |
Tooltips |
Indicates whether data in a table cell should contain
tooltips displaying the content. By default, this check box is
cleared. |
Type |
The data type of an input component. If you are configuring
the settings of an component of the type graph or gauge, this
field contains a list of graph or gauge types. |
Style |
The style of a meter-type gauge component. |
|
Conditions |
The condition based on which the component appears in the
application. For example, you can create a condition that a
control button or a warning image be displayed if the
temperature recorded by the sensor exceeds 40 degrees
Celsius. |
Show on |
The devices wherein the component appears. By default, the
options Mobile, Tablet, and Desktop are selected. |
Hidden |
Indicates whether the component should appear in the
application. By default, this check box is cleared. You can
configure hidden components to appear when an action is
performed. |
|
X-axis Label |
The label of the horizontal axis of an component of the type
graph. |
Y-axis Label |
The label of the vertical axis of an component of the type
graph. |
Required |
Indicates whether it is mandatory to enter a value for the
component that is used as an input to a query. By default, this
check box is cleared. |
Target Data |
The query input that is the target for the value of the
component. |
Source |
The source from which data should be retrieved to initialize
the component. If you are configuring the settings of an input
component, you can select one of the following options:
- Data: Fetches data that from a global variable or the
output value of a query.
- Manual: Allows you to enter a value manually.
- Formula: Allows you to create a formula using global
variables and the output values of a query.
If you are configuring the settings of a display
component, you can select one of the following options:
- Data: Displays data from a global variable or the output
value of a query.
- Manual: Allows you to enter a value manually.
- Formula: Allows you to create a formula using global
variables and output values of a query.
- URL: Displays an image from a URL.
- File: Allows you to upload an image for the
component.
|
Group By |
Enables to group the data in a graph by the selected tag
name. |
Options |
Indicates whether the values in the component are hard-coded
or displayed dynamically from a query. |
Actions |
The action that should be triggered when the component is
selected. |
First Option |
The first option that appears in an component of the type
drop-down list box (for example, select an asset). |
Step |
The step value used for a slider component. |
|
Minimum |
The minimum value for an component that contains a range
(such as a slider or a gauge). |
Maximum |
The maximum value for an component that contains a range
(such as a slider or a gauge). |
True Label |
Customized text that appears when a toggle or an indicator is
active. |
False Label |
Customized text that appears when a toggle or an indicator is
inactive. |
Width |
The width of the component of the type toggle. |
Show <number> rows at a time |
The number of rows that can appear at a time in an component
of the type grid. |
Validation |
The validations to be applied on the value entered in an
input component. You can select the following options:
- Capital: Select this check box if you want application
users to enter a value only in uppercase.
- Minimum character: Select this check box if you want to
set a minimum character limit to values entered in the
component, and then enter the number of minimum
characters that application users must enter in the
component.
- Range Limit: Select this check box if you want to set
the maximum and minimum values that can be entered in a
numeric, date, or time input component.
|
Disabled |
Indicates whether you want the component to appear as
disabled in the application. |
Range Limit |
The range of values that application users can enter in the
component. |
Stacked |
Indicates whether the bars displayed in an component of the
type graph should be stacked. By default, this check box is
cleared. |
Visual |
Rounded Corners |
Applies rounded corners for the selected component. |
Custom Colors |
Select the check box to set these options:
- Add text color.
- Add container background color.
- Add container border color, width, and style.
|
Horizontal Alignment |
Aligns the component left, right, or center. |
Responsive |
Responsive Pattern |
Select how the container layout must respond on web
pages. |