Upload Devices
Using the upload devices widget, you can upload a list of assets to Operations Hub. This data is stored in the baseline M2M entities.
Using the Upload Devices Widget
Column Heading | Purpose | Usage | Mapped to Entity | Mapped to Entity Field |
---|---|---|---|---|
device_unique_name | Identifies the unique ID of the device gateway or asset. This is the ID that the device will use when sending data using REST APIs or MQTT APIs. | This column is required. |
device_gateway | device_id |
M2M_groups_device_thing | gateway_thing_id | |||
device_type | Identifies the type of the device gateway or asset. | This column is required. | device_gateway | device_type |
supported_device_gateway | device_type | |||
unique_address | Identifies the unique address of the device gateway (for example, imei number, mac address, unit ID). | If there is no unique address, enter None. This column is required if the url column is blank. | device_gateway | unique_address |
url | Identifies the URL for the device gateway. | If there is no URL, enter None. This column is required if the unique_address column is blank. | device_gateway | url |
thing_unique_name | This parameter is obsolete. | This column is required and must be blank. | ||
thing_type | This parameter is obsolete. | This column is required and must be blank. | ||
group_name | Identifies the name of the device group. If the group does not exist in Operations Hub, it will be created. | This column is required. If devices are not grouped, we recommend that you enter the same value as in the device_type column. | M2M_groups | group_name |
M2M_groups_device_thing | group_name | |||
group_type | Identifies the group type. The supported group type is gateway. | This column is required. | M2M_groups | group_type |
- Columns mapped to the device_gateway entity:
- device_location
- device_altitude
- device_latitude
- device_longitude
- device_latlong
- device_username
- device_password
- device_firmware_ver
- device_description
- device_generic_1
- device_generic_2
- Columns mapped to the supported_device_gateway entity:
- supported_description
- supported_manufactor
- supported_product_code
- supported_generic_1
- supported_generic_2
- Columns mapped to the M2M_groups entity:
- group_generic_1
- group_generic_2
- group_description