Event Settings
An event settings widget is used to allow users to turn on or off event notifications using the application.
Using the Event Settings Widget to Control an Event
- Create an email template named Temperature_Warning, which you will use to send email notifications.
- Create an event named Temperature_Warning. In the event:
- Create a trigger based on a device.
- Create an action to send an email using the email template that you have created.
Tip: For information on creating an event, refer to the Events section of the documentation. - Using the page designer, add the event settings widget to the relevant page of the application.
- In the EVENT SETTINGS PROPERTIES section, in the Event box, select the event High_Temperature.
- Save the application, and then access it.
The event settings widget appears in the application.
- Select Add new notifier to add an instance of the event.
The Event notifier section appears, displaying the settings that you have configured.
- Change the settings as needed, switch the ON toggle, and then select Create.
The event is now active and will be triggered when the temperature reaches the specified limit.