Date Picker
With the DatePicker plugin, you can add a calendar to display date and time in a variety of formats.
Specify these plugin properties:
Item | Description |
---|---|
Title | Provide the text that appears as a label above the plugin in the end application. |
Type | Select from these options for display in the end application:
|
Display Format | Select the format for the date and time display. |
Timezone | Select the timezone as local or UTC. Note: For Historian sources, use
'local' for timezone. |
Source Input Value | Set this value to allow the plugin to start displaying a specific date
and/or time when it loads in the end application. |
Input Target | This is the value the plugin provides as an output in the end
application. For example, you can choose a date/time/datetime that is passed
to the query, which requires a date time. |