About Applications
- Create all the components that are required for the application.
- Create the pages and dashboards for the application.
- Apply themes, define the navigation details.
- Access and test the application.
- Provide users access to the application.
Suppose you want to create an application that will send an email notification if the temperature recorded by a sensor exceeds 40 degrees Celsius. In this case, you will perform the following tasks:
- Create an email template, which will contain the text and event parameters that you want to send in the email.
- Create an event that will be triggered when the temperature recorded by the sensor exceeds 40 degrees Celsius.
- Add an action to the event to define the recipients and send an email using the email template that you have created.
- Create a page to display the sensor data. You can display the data using components such as text, gauges, or historical trend charts.
- Add an event settings component to the page to allow application users to turn the event on or off.