Troubleshooting USB Hardware Installation

The License Client requires between 20 and 60 seconds to recognize and read a USB hardware key. The USB icon in the footer indicates the status of the hardware key. If no hardware key is detected, the icon is not illuminated. If the hardware key is detected and successfully read, the icon is illuminated. If the key is detected but has not been successfully read and is unable to interact with the License Client, the icon is illuminated with a red slash.
Note:
  • When you plug in the hardware key, an alert message may be displayed indicating that the computer is interacting with the hardware key, and the License Client does not automatically refresh.
  • On some older Windows operating systems, when you plug in the hardware key, there is no indication that the License Client is interacting with the hardware key, and the License Client does not automatically refresh.

    In both of these cases, you may need to click the Refresh Data button on the View Licenses page to display the license information from the hardware key.

Adding a Dependency for hardware keys

If you have startup issues when using a hardware key, you can add a dependency on the hasplms service. If you are using Sentinel, refer to Adding Sentinel Dependency, or if you are using Wibu, refer to Adding Wibu Dependency topic for more information.

For any other Proficy software products starting as a system service (such as iFIX, CIMPLICITY, and Historian) and for the IGS driver, you should add dependency to Proficy Licensing service.