Adding Wibu Dependency

A Wibu dependency ensures that the Wibu and Common Licensing services start up in the correct order.

Before you begin

The Wibu USB drivers must be installed to use this feature.
Note:
When you perform a License Client upgrade that has new drivers, all Wibu dependencies are removed.

Procedure

  1. In License Client, select the Advanced tab.
  2. From the Advanced tab, select Update Application Settings.
  3. Select the Wibu Service tab.
  4. Select Add Wibu Dependency to add the dependency to the service.

Results

The Wibu Service dependency was added successfully message is displayed.