Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / ServerHostName Property


ServerHostName Property
A fully qualified host name of a Historian server. Due to security identity checks, it is not possible to connect simply via server IP address.

Default is local server if unspecified.

Syntax
Public Property ServerHostName As System.String
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also