Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector.Property Enumeration


In This Topic
    Collector.Property Enumeration
    In This Topic
    Uniquely identifies Historian collector properties.
    Syntax
    Public Enum Collector.Property 
       Inherits System.Enum
    public enum Collector.Property : System.Enum 
    public enum class Collector.Property : public System.Enum 
    Members
    MemberDescription
    CanBrowseSourceWhether a collector can browse source. See Collector.CanBrowseSource.
    CanSourceTimestampWhether a collector can obtain sample times from a data source. See Collector.CanSourceTimestamp.
    CollectionDelayCollector collection delay. See Collector.CollectionDelay.
    CommentCollector comment. See Collector.Comment.
    ComputerNameCollector host computer name. See Collector.ComputerName.
    DataRecoveryQueueEnabledWhether data recovery queue is enabled. See Collector.DataRecoveryQueueEnabled.
    DefaultAbsoluteDeadbandDefault tag absolute collector compression deadband value. See Collector.DefaultAbsoluteDeadband.
    DefaultAbsoluteDeadbandingWhether default collector compression deadband is expressed as an absolute value. See Collector.DefaultAbsoluteDeadbanding.
    DefaultCollectionIntervalDefault tag collection interval. See Collector.DefaultCollectionInterval.
    DefaultCollectionTypeDefault tag collection type. See Collector.DefaultCollectionType.
    DefaultCompressionDefault tag collector compression. See Collector.DefaultCompression.
    DefaultCompressionDeadbandDefault tag collector compression deadband value. See Collector.DefaultCompressionDeadband.
    DefaultCompressionTimeoutDefault tag collector compression timeout. See Collector.DefaultCompressionTimeout.
    DefaultLoadBalancingDefault tag load balancing. See Collector.DefaultLoadBalancing.
    DefaultSpikeIntervalCollector tag spike logic interval. See Collector.DefaultSpikeInterval.
    DefaultSpikeLogicDefault tag spike logic. See Collector.DefaultSpikeLogic.
    DefaultSpikeMultiplierDefault tag spike logic multiplier. See Collector.DefaultSpikeMultiplier.
    DefaultTagPrefixDefault tag prefix. See Collector.DefaultTagPrefix.
    DefaultTimeStampTypeDefault tag timestamp type. See Collector.DefaultTimeStampType.
    DescriptionCollector description. See Collector.Description.
    DisableOnTheFlyTagChangesWhether a collector restart is required to apply configuration changes. Collector.DisableOnTheFlyTagChanges.
    General1Collector general 1. See Collector.General1.
    General2Collector general 2. See Collector.General2.
    General3Collector general 3. See Collector.General3.
    General4Collector general 4. See Collector.General4.
    General5Collector general 5. See Collector.General5.
    HeartbeatOutputAddressCollector heartbeat output address. See Collector.HeartbeatOutputAddress.
    LastModifiedCollector last modified time. See Collector.LastModified.
    LastModifiedUserCollector last modified user. See Collector.LastModifiedUser.
    MaximumMemoryBufferSizeCollector maximum memory-buffer size. See Collector.MaximumMemoryBufferSize.
    MinimumDiskFreeBufferSizeCollector minimum disk free buffer size. See Collector.MinimumDiskFreeBufferSize.
    NameCollector name. See Collector.Name.
    RateOutputAddressCollector rate output address. See Collector.RateOutputAddress.
    RedundancyEnabledWhether collector redundancy is enabled. See Collector.RedundancyEnabled.
    RedundancyFailoverOnBadQualityWhether a collector should automatically failover based on watchdog bad quality. See Collector.RedundancyFailoverOnBadQuality.
    RedundancyFailoverOnCollectorStatusWhether a collector should automatically failover based on collector status. See Collector.RedundancyFailoverOnCollectorStatus.
    RedundancyFailoverOnValueWhether a collector should automatically failover based on specific watchdog value. See Collector.RedundancyFailoverOnValue.
    RedundancyFailoverValueChangeTypeCollector redundancy watchdog tag value monitoring type. See Collector.RedundancyFailoverValueChangeType.
    RedundancyIsActiveCollectorWhether a collector is current active in a redundancy configuration. See Collector.RedundancyIsActiveCollector.
    RedundancyPrincipalCollectorCollector redundancy principal collector name. See Collector.RedundancyPrincipalCollector.
    RedundancyValueMaxUnchangedPeriodCollector redundancy watchdog tag max unchanged period. See Collector.RedundancyValueMaxUnchangedPeriod.
    RedundancyWatchdogTagNameCollector watchdog tag name. See Collector.RedundancyWatchdogTagName.
    ShouldAdjustTimeWhether a collector should adjust time. See Collector.ShouldAdjustTime.
    ShouldQueueWritesWhether a collector should queue data writes. See Collector.ShouldQueueWrites.
    SourceTimeInLocalTimeWhether source times are in local time. See Collector.SourceTimeInLocalTime.
    StatusCollector status. See Collector.Status.
    StatusOutputAddressCollector status output address. See Collector.StatusOutputAddress.
    TypeCollector type. See Collector.Type.
    Version 
    Inheritance Hierarchy

    System.Object
       System.ValueType
          System.Enum
             Proficy.Historian.ClientAccess.API.Collector.Property

    Requirements

    Target Platforms: Windows 98, Windows NT 4.0, Windows Millennium Edition, Windows XP Home Edition, Windows XP Professional, Windows Server 2003 family, Windows Vista, Windows Server 2008 family

    See Also