Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxDepth Property


In This Topic
    XmlReaderQuotaMaxDepth Property
    In This Topic
    Maximum nested XML node depth. Limits the XML nested node depth. Default value is 32.
    Syntax
    Public Property XmlReaderQuotaMaxDepth As System.Integer
    public System.int XmlReaderQuotaMaxDepth {get; set;}
    public:
    property System.int XmlReaderQuotaMaxDepth {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also