Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / SendTimeout Property


In This Topic
    SendTimeout Property
    In This Topic
    Maximum amount of time to send a request before timing out. Default value is 1 minute.
    Syntax
    Public Property SendTimeout As System.TimeSpan
    public System.TimeSpan SendTimeout {get; set;}
    public:
    property System.TimeSpan SendTimeout {
       System.TimeSpan get();
       void set (    System.TimeSpan value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also