Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class
Members


In This Topic
    AlarmInfo Class
    In This Topic
    Represents details of the AlarmInfo Object.
    Syntax
    Public Class AlarmInfo 
    public class AlarmInfo 
    public ref class AlarmInfo 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.AlarmInfo

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also