Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiField Class
Members


In This Topic
    MultiField Class
    In This Topic
    This is the definition of the object contained in the UserDefinedType class.
    Syntax
    Public Class MultiField 
    public class MultiField 
    public ref class MultiField 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.MultiField

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also