Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / ServerCertificateValidationMode Property


In This Topic
    ServerCertificateValidationMode Property
    In This Topic
    A method of validating a security certificate on a Historian server.

    Default is CertificateValidationMode.ChainTrust, a certificate is considered valid if the chain builds to certification authority in the trusted root store.

    Use CertificateValidationMode.None, to connect to a Historian server secured by a self-signed certificate (out-of-the-box configuration).

    Syntax
    Public Property ServerCertificateValidationMode As CertificateValidationMode
    public CertificateValidationMode ServerCertificateValidationMode {get; set;}
    public:
    property CertificateValidationMode ServerCertificateValidationMode {
       CertificateValidationMode get();
       void set (    CertificateValidationMode value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also