Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxNameTableCharCount Property


In This Topic
    XmlReaderQuotaMaxNameTableCharCount Property
    In This Topic
    Maximum size of character data in a reader's NameTable. Default value is 16K.
    Syntax
    Public Property XmlReaderQuotaMaxNameTableCharCount As System.Integer
    public System.int XmlReaderQuotaMaxNameTableCharCount {get; set;}
    public:
    property System.int XmlReaderQuotaMaxNameTableCharCount {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also