February 28, 2019
- SeaStream DP will enable the ship to perform operations with stability, safety and precision for a long time.
- The “Energy Efficient” mode of the DP system can help reduce fuel consumption by up to 10%
- GE has partnered with multiple universities in Korea to provide DP systems in recent years
BUSAN – 28 February 2019 - Pukyong National University (PKNU) has chosen GE’s Power Conversion business to provide the SeaStream Dynamic Positioning (DP) system for their training vessel for fisheries industry training. GE’s SeaStream DP will enable the ship to perform operations – for example controlling horizontal movement or holding position against harsh wind and in choppy waters – with stability, safety and precision for a long time.
“We have more than six decades of onboard vessel training experience and are now adding a 14th vessel to the fleet. We are glad to work with GE, whose robust technology will contribute to us adding the largest and best equipped new vessel to our fleet,” said Professor LEE JONG-GUN, director of the PKNU Ship Training and Operations Center, PKNU.
SeaStream DP is also a smart system that will contribute to the ship’s overall efficiency and operational effectiveness.
The “Energy Efficient” mode of the DP system can help reduce fuel consumption. The position and heading of the vessel are both controlled automatically, predictive software is used to anticipate position variation and to limit thrust changes if the vessel is predicted to remain within the so-called ‘soft’ operating window, or an inner tolerance band. If the vessel is predicted to move outside its ‘hard’ operating window (outer tolerance band), the system develops optimum thrust to remain within that window. Advanced algorithms are used to optimize vessel heading to further reduce power consumption and limit thruster/machinery wear and tear.
GE studies have shown that fuel saving in this mode may be up to 10 percent or more, with an associated NOx reduction of up to 20 percent, depending on environmental factors and exact operational profile.
“GE’s DP system is more mariner friendly, which is an excellent choice for fishery training purposes. With an informative and easily-operable human-machine interface, the system provides unprecedented flexibility and effectiveness that allows operators to truly focus on their maritime operations,” said Ed Torres, CEO of marine and oil & gas, GE’s Power Conversion business.
“We have partnered with multiple universities in Korea to provide DP systems in recent years, helping to train students with valuable skills and to fuel their ambition to pursue a successful career at sea,” said Azeez Mohammed, president & CEO, GE’s Power Conversion business. “We are excited to be part of the journey, helping the next generation of maritime professionals excel with one of the most advanced technologies for efficient ship operations.”
Built by DAE SUN Shipbuilding & Engineering Co. Ltd, the training ship is 97 m long and 15.4 m wide. It has a gross tonnage of 3,990 ton and a capacity of 160 people.
About GE
GE (NYSE:GE) drives the world forward by tackling its biggest challenges: Energy, health, transportation—the essentials of modern life. By combining world-class engineering with software and analytics, GE helps the world work more efficiently, reliably, and safely. For more than 125 years, GE has invented the future of industry, and today it leads new paradigms in additive manufacturing, materials science, and data analytics. GE people are global, diverse and dedicated, operating with the highest integrity and passion to fulfill GE’s mission and deliver for our customers. www.gevernova.com
About GE Power
GE Power is a world energy leader providing equipment, solutions and services across the energy value chain from generation to consumption. Operating in more than 180 countries, our technology produces a third of the world’s electricity, equips 90 percent of power transmission utilities worldwide, and our software manages more than forty percent of the world’s energy. Through relentless innovation and continuous partnership with our customers, we are developing the energy technologies of the future and improving the power networks we depend on today. For more information please visit www.gevernova.com/power, and follow GE Power on Twitter and on LinkedIn.
For more information, contact: Kate Inglis, GE Power Conversion, +44 (0) 1788 563386, +44 (0) 7766 991040, kate.inglis@ge.com