Full electrical solution for FPSO

Variable-Speed Drive Systems (VSDS) for topside and subsea motors - CLOV Offshore, Angola Oilfields

 

The Case

A new development pole in Angola
CLOV is the fourth development pole in Angola’s deep offshore Block 17, which is operated by Total. Also known as the “Golden Block,” Block 17 covers nearly 4,000 square kilometers, from 150 km to 270 km off the coast . CLOV is a stand-alone development in a four-field cluster consisting of the oilfields Cravo, Lirio, Orquidea and Violeta. These oilfields contain reserves of 505 million barrels of oil at a water depth of 1,050 m to 1,400 m.

The first full electrical FPSO
GE’s Power Conversion business was awarded a contract to supply seven complete VSDS, including induction motors, for the main gas compressors and the water injection pumps, as well as two VSDS for subsea multiphase pumps. This project represents the first floating, production, storage and offloading unit to be fully equipped with electric variable-speed drive equipment. The total electrical power is about 50 MW.

Feeding subsea equipment
The transformers and MV7000 converters installed topside feed the subsea multiphase pump induction motors through 11 km umbilical. Power Conversion’s advanced converter control allows for driving a motor with a step-up transformer and long step-out distance between the subsea motor and the topside converter.

 

Our solution

Four complete VSDS for the high-pressure compressor units, each comprised of :

  • Step-down transformer
  • Medium-voltage MV7000 converter
  • 9.61 MW induction motor 6 kV/1,717 rpm

One complete VSDS for low-pressure compressor unit comprised of :

  • Step-down transformer
  • Medium-voltage MV7000 converter
  • 4.89 MW induction motor 6 kV/1,717 rpm

Two complete VSDS for water injection pumps, each comprised of :

  • Step-down transformer
  • Medium-voltage MV7000 converter
  • 8.7 MW induction motor 3 kV/1,900 rpm

For the subsea multiphase pumps :

  • Step-down and step-up transformers
  • Two medium-voltage MV7000 converters feeding a 2.3 MW induction motor 6 kV/3,797 rpm

 

The challenge

Because the project calls for in-depth facilities and production techniques, the customer required high-performing, reliable and efficient systems that would help optimize production in a space-constrained environment. With those key drivers in mind, Power Conversion designed and provided a compact and lightweight electrical solution based on proven, high-performance technologies for the offshore facility’s pumps and compressors.

Feeding topside equipment
Transformers and MV7000 converters, which are feeding induction motors, have been installed topside for the high- and low-pressure compressor units and water injection pumps. Their compact design allows for a smaller electrical room. Thanks to the converter 24-pulse topology for network bridge, no harmonic filter is necessary, thus allowing an additional reduction of the equipment footprint and capital expenditures. By using a 6 kV converter, the size and weight of cables between the motor and the converter also are decreased by half.

Medium-voltage converters bring high- quality performance
With the most compact design available for a medium-voltage converter, Power Conversion’s high-performance MV7000 solution is based on the latest generation of powerful press-pack IGBT (PPI) technology. The proven Pulse Width Modulation (PWM) three-level inverter provides high-quality performance. Its adjustable PWM patterns and frequency bring a wide range of flexibility for low switching losses, low motor total harmonic distortion, operation at high frequency up to 300 Hz or at long distance, and negligible amplitude of torque pulsation at the motor shaft.

The compressors, water injection pumps and subsea pumps for CLOV are powered by the MV7000 converter series. Their water-cooled design, ideal in a space-constrained environment such as offshore applications, allows for reduced investment in room ventilation and air conditioning. In addition, it makes the use of high-capacity diodes and PPI optimal versus footprint . Water-cooling converters also operate with very low noise.

Powerful medium-voltage induction motors
Our medium-voltage induction motors offer lower weight and inertia advantages as well as lower maintenance costs for applications requiring high reliability.
They are available on any type of drive system for most industrial applications, including FPSOs. These machines also offer higher overload capacity and represent a more cost-effective solution compared to equivalent synchronous machines.

Induction motors supplied for CLOV provide the following benefits :

  • More complete plant safety with pressurized Expx IIAT3 motor
  • High efficiency with a direct-drive gearless solution
  • Optimized footprint thanks to water-cooled technology
  • Smooth startup with variable-speed drive control
  • Operating expenditure savings with reduced maintenance service

In addition to routine tests on each item of the VSDS, the system (including the cooling system) has been tested at rated power (full speed, full load) prior to installation.