Turn data items into parameters

Before you begin

Note: Parameterized data items defined on a subprocess must be bound to data items defined on a workflow when the subprocess is added to a workflow.
Attributes include:
  • parameters
  • local variables
  • data items
  • external events
  • namespaces
A resource must already have been added in order to select it from this list. For more information, see Add a resource to the workflow model.

Procedure

  1. In the navigator, click Workflow.
  2. In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
  3. In the resource type list, select a resource.
  4. In the Displays panel, click Workflow Management > Workflow Editor.
  5. Click the Workflow Editor tab.
  6. To configure a workflow, from the workflow configuration panel, click Edit next to the attributes collection you want to work with.
  7. To configure a subprocess:
    1. Double-click the subprocess you want to work with.
    2. From the subprocess configuration panel, click Edit next to the attributes collection you want to work with.
  8. Optional: To change this value at run time, use a Write Activity.
  9. In the Edit dialog box, click Add.
    Tip: See section on each attribute for configuration.
  10. From the Data Items list, select the item you want to work with.
  11. From the Details list, select the Make this data item a parameter check box.
  12. Click OK, and then click Save.