Local Variables

Local variables are used as local data sources that are available to the running workflow during the lifetime of the workflow instance.

Local variables can be written to by an activity bind or from a Write activity. For example, you have a workflow with a subprocess called Subprocess1, and the subprocess contains two activities: Activity1 and Activity2. Subprocess1 also contains a local variable called Variable1. When the workflow runs and reaches Subprocess1, Activity1 writes to Variable1. Activity2 can now read from Variable1, and Variable1 can be manipulated depending on the type of activity that Activity2 is defined as.

Local variables can be defined at both the workflow and subprocess levels. Subprocess local variables can be accessed only from within the specific subprocess they were created in, whereas workflow level local variables can be accessed from anywhere within the workflow. For example, an activity in one subprocess can write to a workflow local variable, and in turn be accessed again in another subprocess.
Tip:
You can use a Write Activity to change some property values at run time.

Local Variable Properties

The following table describes the available options.

AttributeValueDescription
ListN/ADisplays the items created for the current workflow or subprocess.
AddN/AClick to add.
RemoveN/AClick to delete the selection.
NameUser-definedSpecifies a display name for the selected property.
TypeUser-definedSpecifies the data type for the variable.
Initial ValueUser-definedSpecifies a value that corresponds with the data type specifications.
Allow tracking for this variableN/ASelect this check box to add the local variable to a trackable variables list in Tracking Configuration, and to ensure that data related to a task is available when a running workflow completes.
Important:
To track a variable, you must also select it in Trackable Variables in the Tracking Configuration tab.
Note:
To view a tracked variable after a workflow has run, enable tracking at both the process (workflow) and subprocess level.
DescriptionUser-definedProvides more information that a user may find helpful.