Work Instructions

The Work Instructions tab is where you can input detailed instructions for a person performing a task or task step.

These instructions appear as a Work Instructions button in the Task List. If no information is available, this section is not visible to an operator. The information can include anything that an operator requires to perform a workflow task or a subprocess task step, or finds useful to complete the task/task step.

Note:
If content in the work instructions area exceeds a certain threshold, the editor may not perform optimally during design time, as well as in the Task List during run time. To prevent this issue, use the following recommendations: use small graphic files; use small amounts of text, or several line breaks, within the body of the work instructions area.

Updating Work Instructions During Run Time

You can use keywords to replace text in work instructions and email subjects and bodies. This text is replaced with keyword values in a workflow at run time.

For more information, see Replace keyword text during run time.

Attributes

The following table describes the available options.

AttributeValueDescription
Task/Task Steps listN/ASpecifies the name of the currently selected workflow, and the names of all subprocesses associated with that workflow.
Work InstructionsUser-definedSelect the workflow or a subprocess, and then enter instructions related to that task or task step.