Delete a web service definition

If your web service definition is not being used by a running workflow instance, you can delete it.

About this task

You can delete a web service that is configured for use in a non-running workflow; however, when that workflow is loaded in the Workflow Editor, a validation error is displayed indicating that the workflow uses a connection that no longer exists. You cannot delete a web service definition that is being used in a running workflow instance.

If any Silverlight form is configured to use a server method that is associated with a deleted web service, then an error message is displayed in the Feedback Zone. If the same server method contains a complex data type, you cannot configure that method again; the method must be deleted from the form, added again, and then configured.

Procedure

  1. In the navigator, click Proficy System > Proficy System > Web Services.
  2. From the Web Service Definition list, select the web service you want to remove.
  3. Click Delete, and then click OK.