Add a web services definition
A web service definition must point to a valid WSDL file that contains all of the endpoints and methods you want to use for the web service. You can create multiple web service definitions, each pointing to a different WSDL URL.
Before you begin
You must have a web service with valid WSDL running before you can add a web service in Workflow using the Web Services Service Provider.
In order to manage web services, you must be a member of a personnel group that has the Manage Web Service key set permission assigned to it.
Web service complex types can be instantiated and initialized using the Code activity. A namespace related to a web service has to be added in the Namespace Browser in the Workflow Editor when configuring a workflow.
About this task
Procedure
- In the navigator, click .
- Click Add Web Service.
- In the Name field, enter a unique name for the web service.Namespace details are automatically populated in the Namespace field.
- In the WSDL URL field, enter the address of the WSDL file you want to associate with the web service.
- In the Description field, enter more information related to the web service.
- To change the preconfigured string in the Namespace field, enter a new namespace using C# namespace guidelines.The appropriate namespace prefix is Proficy.WebServices. .
- Click OK.Note:If the web service interfaces and methods do not appear in the Silverlight forms editor, then you must restart the Workflow client.