Configure endpoints for a web service
Endpoints are used to connect to a web service.
Before you begin
In order to manage web services, you must be a member of a personnel group that has the Manage Web Service key set permission assigned to it.
About this task
Important:
If the web service is not licensed (as indicated by the message in the License Overview area), then you cannot execute any of the methods contained in the WSDL file.
Procedure
- In the navigator, click .
- From the Web Service Definition list, select the web service you want to work with.
- In the Displays panel, click Web Service Editor.
- Click the Overview tab.
- In the Endpoint field, select an endpoint you want the web service to use for communications.
- In the Location URL field, change the address of the WSDL file only if one of the following has occurred:
- The web service has been moved to a different server.
- The server is renamed.
- The web service is hosted at a different URL.
- Depending on the authentication scheme the web service uses, do one of the following:
If the authentication scheme uses... Then, do this... User Credentials - In the User Name field, enter a valid user name.
- In the Password field, enter the password for the user.
Certificate Credentials - In the Store Location field, select the location of the X.509 certificate store you want to use.
- In the Store Name field, select the name of the X.509 certificate store you want to use.
- In the X509 Find Type field, enter the value you want the X509Certificate2Collection.Find method to search for.
- In the X509 Find Value field, select the value you want the X509Certificate2Collection.Find method to search for.
Note:If the endpoint is configured to use the user name and password details, then in order to test or use this endpoint, you must enter valid information in these fields. - Repeat steps 5-6 for each endpoint to configure for the web service.
- Click Save.