Create a simple web form with images

You can use the Designer to create basic HTML forms with simple images, such as a logo.

About this task

Note:
You can create HTML forms for use only in the Workflow client Task List and in the Mobile Task List.

Procedure

  1. In the navigator, click Global Displays.
  2. From the Forms folder, add a new form, or select a form from the Forms list.
  3. In the Displays panel, click Display Editor.
  4. On the Overview tab, select Use the Designer tab to create a simple web form.
  5. Click Save.
  6. Click the Designer tab.
  7. In the Form Fields section, click the Image form control to add the field to your form.
    You can add multiple image fields, as well as other form controls. Each image is labelled and numbered in the Name field in sequence; for example, Image1, Image2, and so on.
    The Layout area displays the basic configuration for your form.
  8. Optional: To move fields around the Layout area, select the field to drag and drop it to a different location within the panel.
  9. Optional: To delete a field, select it, and then click Delete.
  10. In the Properties section, you can configure the form fields.
    1. In the Name field, enter a unique identifier by modifying the existing text.
      You can view the name of the field property when you add a Form activity to a workflow in the Workflow Editor. You can then bind a value to this property.
    2. In the Label field, enter descriptive text on the form control that is displayed to the operator.
    3. In the URL field, enter the absolute path of the image's location.
    4. In the Alignment field, from the drop-down list, select an alignment value.
      • Left
      • Center
      • Right
    5. In the Height field, enter a whole number to represent the number of pixels for the height of the image.
      Note:
      If no value is specified, the default dimensions are used.
    6. In the Width field, enter a whole number to represent the number of pixels for the width of the image.
      Note:
      If no value is specified, the default dimensions are used.
  11. Click Save.