Images in Web Forms

You can use the Designer to create basic HTML forms with simple images, such as a logo.

Properties

AttributeValueDescription
NameUser-defined alphanumeric string (A-Z, a-z, 0-9)Specifies a unique identifier that is displayed in a workflow's Form activity. You can then bind properties associated with the selected form field.
LabelUser-defined alphanumeric string (A-Z, a-z, 0-9)Specifies descriptive text on the form control that is displayed to the operator.
URLUser-defined alphanumeric string (A-Z, a-z, 0-9)Specifies the web address where the image is located.
Note:
This path must be accessible by the machine that the operator is working on during run time.
AlignmentUser-definedSpecifies the location of the text in the form, such as left, right, or center.
HeightUser-defined numeric valueSpecifies the height in pixels.
WidthUser-defined numeric valueSpecifies the width in pixels.