Requirements for Creating Custom Web Forms
You can create custom web forms, and then bind, build an expression, or set a literal value against the input and output parameters in a workflow.
Form Library
All custom web forms must include the form library, which is contained in tasklistform.min.js via a script tag (for example, <script src="https://<Insert Host Name Here>/tasklistform.min.js"></script>). This file is located in <32-bit installdir>:\Program\Applications\Workflow\SDK. You can also find a file that provides information about calling the required functions that allow forms to work in the Task List.
Custom Form Template
The file, FormTemplate.html, provides information about calling the required functions that allow forms to work in the Task List. This file is located in <32-bit installdir>:\Program\Applications\Workflow\SDK.
Communicating with the Task List
- formLoaded() when it is ready to receive input data; for example, in the onloaded event of your body element
- submitForm() to perform a submission back to workflow; for example, in the onsubmit handler of your form element
- cancelForm() when it wishes to signal a cancellation of the form; for example, in the onclick handler of a cancel button)
For examples of how these calls are performed, see the included sample form.
Using Custom Web Forms in the Workflow Task List
In order for custom HTML forms to function properly in the regular Task List, you must ensure the following line is added at the start of the <head> section of your form.
<meta http-equiv="X-UA-Compatible" content="IE=Edge,chrome=1">
Hosting Sample Files
<link rel="stylesheet" type="text/css" media="screen" href="https://<Insert Host Name Here>/SampleForm/css/jquery-ui.css"/>
<link rel="stylesheet" type="text/css" media="screen" href="https://<Insert Host Name Here>/SampleForm/css/ui.jqgrid.css"/>
<script src="https://<Insert Host Name Here>/SampleForm/js/jquery-1.11.0.min.js"></script>
<script src="https://<Insert Host Name Here>/SampleForm/js/i18n/grid.locale-en.js"></script>
<script src="https://<Insert Host Name Here>/SampleForm/js/jquery.jqGrid.src.js"></script>
<script src="https://<Insert Host Name Here>/SampleForm/js/jquery-ui.js"></script>
<script src="https://<Insert Host Name Here>/SampleForm/js/tasklistform.min.js"></script>
Accessing Custom Web Forms
Customers who create custom web forms must also provide secure web hosting in order for these forms to be accessible by Workflow. As a result, you must use an HTTPS address. When you configure a custom web form, use only this HTTPS address in the URL field.
To use a custom HTML form with the Web HMI Task List, Web HMI must be configured to allow connections to the custom form host.
- Open the C:\Program Files\Proficy\ProficyWebServer\ReverseProxy\serverConfig.json file on the Web HMI Server.
- Edit the whitelist element to include the custom form host. e.g.,
"whitelist" : [ "https://myformhost:port" ],
- Restart the “GE Proxy” windows service.
Form Events in Web-based Forms
For more information on using form events, see Event Handlers for Web-based Forms.
Requirements for Binding Input and Output Parameters
- There must be exactly one <form> element in the custom HTML.
- All elements must have a unique Name attribute. Note:Exception for radio buttons: All radio buttons in a radio group have the same name.
- Labels: The For attribute must be set to the ID of the corresponding element.Note:Exception for radio buttons: Labels for radio groups have the Name property set to the same Name of each radio button. A label element must be present to ensure that the radio button options can be modified from a running workflow.
- Authentication: For custom web forms to work properly, there must be no authentication on the server hosting these forms.
- Modifying forms: If you make changes to the custom form, you must save it in order for the changes to work.
- To tell the host which methods to call when passing in the initial workflow inputs and when collecting the form outputs to return, the form must call addInputParameterFunction and addOutputParameterFunction. This call is handled automatically for most basic HTML elements, such as <p>, <input>, <textarea>, <select>, and <img>.
- Inputs:
- Add an input parameter function with the string name <elementName>.InitialValue for each control input that you want to handle.
- In the sample form, the jqGrid populates using a JSON representation of a table:
if (addInputParameterFunction) { addInputParameterFunction('jqGrid.InitialValue', populateForm); }
- Outputs:
- Add an output parameter function with the name <elementName>.Value for each control output that you want to provide. Returns a string.
- In the sample form, a JSON representation of the table is returned:
if (addOutputParameterFunction) { addOutputParameterFunction(collectFormOutput); }
Supported Binding Elements
Control | Tag | Element |
---|---|---|
Text | <p> |
|
Image | <img> |
|
Input | <input> |
|
Selection | <select> |
|
Radio Buttons | <input> |
|
List Box | <select multiple> |
|
Others | N/A |
|