Check Boxes in Web Forms
You can use the Designer to create basic HTML forms with check boxes.
Properties
Attribute | Value | Description |
---|---|---|
Name | User-defined alphanumeric string (A-Z, a-z, 0-9) | Specifies a unique identifier that is displayed in a workflow's Form activity. You can then bind properties associated with the selected form field. |
Label | User-defined alphanumeric string (A-Z, a-z, 0-9) | Specifies descriptive text on the form control that is displayed to the operator. |
Required | User-defined; Boolean | Select one of the following options:
|
Auto Check | User-defined; Boolean | Select one of the following options:
|