Combo Boxes in Web Forms
You can use the Designer to create basic HTML forms with combo boxes.
Properties
Attribute | Value | Description |
---|---|---|
Name | User-defined alphanumeric string (A-Z, a-z, 0-9) | Specifies a unique identifier that is displayed in a workflow's Form activity. You can then bind properties associated with the selected form field. |
Label | User-defined alphanumeric string (A-Z, a-z, 0-9) | Specifies descriptive text on the form control that is displayed to the operator. |
Options | User-defined; String | Required; Specifies the values for each form field line that are viewable to an operator during run time as a drop-down list. |
Default Option | User-defined; String | Optional; From the list of options for the control, select the one that you want the operator to interact with first. |