Create a material property aspect
Before you begin
Note:
Activities can be inserted at both the workflow and subprocess levels.
About this task
Material property aspects dynamically extend material definition instance or class properties without modifying or recompiling the original objects.
Procedure
- In the navigator, click .
- In the Workflows list, select the resource you want to work with.Note:A resource must already have been added in order to select it from this list.
- In the Displays panel, click .
- Click the Workflow Editor tab.
- Insert an activity:
- At the workflow level:
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.Note:Activities can exist only between the presubprocess and postsubprocess.
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
- At the subprocess level:
- Double-click the local subprocess you want to add the activity to.
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
- At the workflow level:
- On the activity configuration panel, click Configure Method.The Configure Method dialog box appears, displaying a list of the available call method service providers.
- Double-click IMaterial to display the list of available call methods.
- Click AddPropertyAspect, and then click Finish.The input parameters appear in the activity configuration panel.
- Configure the call method as follows:
- In the Aspect Name field, enter the name of the aspect you want to add to the resource.
- In the Material field, click the ellipsis button, and then select a class or definition.
- In the Property Name field, enter the name of the property you want to add the property aspect to.
- Click Save.
- Run the workflow, or, on the Test/Debug tab, test the workflow to ensure that your input parameters are configured correctly.