RemoveClass (IMaterial)

Removes a specified material class from a specified material definition.

InputsData TypeDescription
materialClassDirectoryResource

Specifies the name of the material class to remove from the material definition.

materialDefinitionDirectoryResource

Specifies the material definition to remove the class from.

Note:
In the Configure Method dialog box, click Next to select a resource. Otherwise, in the Inputs section of the activity configuration panel, click the ellipsis button to select a resource.