AddPropertyAspect (IMaterial)
Adds an aspect to a material definition or class property.
Inputs | Data Type | Description |
---|---|---|
aspectName | String | Specifies the property aspect to associate with the property. |
material | DirectoryResource |
Specifies the material definition or class to add the property aspect to. |
propertyName | String | Specifies the name of the property to add the aspect to. |
Note:
In the Configure Method dialog box, click Next to select a resource. Otherwise, in the Inputs section of the activity configuration panel, click the ellipsis button to select a resource.