RemovePropertyAspect (IMaterial)

Removes an aspect from a property owned by a material definition or material class.

InputsData TypeDescription
aspectNameString

Specifies the name of the aspect type to remove.

materialDirectoryResource

Specifies the material definition or class to remove the aspect from.

propertyNameString

Specifies the name of the property to remove the aspect from.

Note:
In the Configure Method dialog box, click Next to select a resource. Otherwise, in the Inputs section of the activity configuration panel, click the ellipsis button to select a resource.