Add custom configuration to a template

Workflow Designers can specify additional custom configuration information for the selected template within the Template Editor.

Procedure

  1. In the navigator, click eSOP > Task Templates.
  2. In the resource list, add a resource, or select the resource that you want to work with.
  3. In the Displays panel, click Template Editor.
  4. To add custom configuration information, on the Metadata tab, click Add.
    1. In the Name column, double-click inside the table cell to modify the name.
    2. In the Metadata column, double-click inside the table cell to enter a value that has a maximum length of 4000 characters.
    3. To delete an existing row, select it, and then click Remove.
  5. Click Save.