Config Panel Editor

You use the Config Panel Editor to create custom configuration panels. These panels are based on existing forms or user displays that have been created in Workflow.

PropertyValueDescription
.NET or Silverlight AssemblyUser-definedClick Set to locate and select the assembly that contains the display you want to add.
Class NameUser-definedSpecifies the class name of the display contained by the selected assembly.

Template Editor

You can configure panels for both the task and task step level. After you add the assembly in the Config Panel Editor, you can further manipulate the order of the panels in the Template Editor. The outcome of these configurations are displayed in the Task Editor and viewed by the person constructing tasks.