Template Editor
You use the Template Editor to associate a workflow with a template, customize preconfigured user controls, and indicate specific text to be replaced with live values during workflow run time.
Set Templates
Workflow Designers create workflows to be used as eSOP task templates. You must first define the workflow and configure the template options.
Property | Value | Description |
---|---|---|
Set | N/A | Click to select an existing workflow. |
Template Type | N/A | From the drop-down menu, select one of the following template type to associate with your workflow template.
|
Custom Configuration Panels
You can configure panels for both the task and task step level. After you add the assembly in the Config Panel Editor, you can further manipulate the order of the panels in the Template Editor. The outcome of these configurations are displayed in the Task Editor and viewed by the person constructing tasks.
Property | Value | Description |
---|---|---|
Add Property | N/A | Click to add a configuration panel resource from Config Panels. This resource is then displayed as tabs in the Task Editor for the Task Builder. |
Remove | N/A | Click to remove a configuration panel resource from the table. |
N/A | Click the up or down arrow to change the order that the tabs are displayed in the Task Editor for the Task Builder. | |
Order | User-defined | Click the selected table row to move the tab that appears in the Task Editor moves further to the left in the display. |
Tab Name | User-defined | Specifies the name attributed to the configuration panel resource created in Config Panels. To change the name of the tab as it appears in the Task Editor, double-click the table cell, and enter new text. |
Configuration | User-defined | Specifies additional custom configuration information for a panel. To add or modify content, double-click the table cell, and then add .csv or .dita text to customize a particular configuration panel instance. |
Config Panel | User-defined | Specifies the name of the configuration panel resource from Config Panels. |