Task Editor Grid

The Task Editor is a starting point for building tasks that will be used in running workflows. Using this editor, you create and manage the configuration data in the task you are building.

Task Information Grid Headings

You can see task information displayed in a grid for easy viewing. To add or modify task information, including adding a task step to a task, click the Edit button.

AttributesValueDescription
TaskUser-definedSpecifies a unique name assigned to a task.
Display NameUser-definedSpecifies a name given to a workflow task for the user to see during run time.
DescriptionUser-defined up to 255 charactersProvides more information about a resource that a user may find helpful.
GroupUser-definedSpecifies a group name for managing similar tasks. You can sort tasks based on their group. Click the drop-down arrow to select an existing group.

General Controls

When you view task information in the Task Editor, several controls are available to work with the tasks.

ButtonValueDescription
Edit OR TasksN/AClick the Edit button to enter the configuration section for a task or task step. Click the Tasks button to view tasks in a table format.
AddN/AClick to add a new task.
DuplicateN/AClick to re-create an existing task.
DeleteN/AClick to delete the selected existing task.