Basic Settings for Building Tasks

The Task Editor is a starting point for building tasks that will be used in running workflows. Using this editor, you create and manage the configuration data in the task you are building.

Insert More Task Steps

You can add more task steps to a task. The number of steps you can add is predetermined by the template.

AttributesValueDescription
Add StepN/AClick to add a task step to a step.
Delete StepN/AClick to remove a task step from the selected step.

Details Tab - General Information

To add data to a task, including adding subprocess task steps, you select a specific task that has already been entered into the system. To view task information in a table, click the Tasks button.

AttributesValueDescription
NameUser-definedSpecifies a unique name assigned to a task.
Display NameUser-defined Workflow levelSpecifies a name given to a workflow task for the user to see during run time.
DescriptionUser-defined up to 255 charactersProvides more information about a resource that a user may find helpful.
ExpirationUser-definedUse the up and down arrows to enter an expiration day or time (hours, minutes, seconds).
PriorityUser-definedSpecifies the importance of a task by indicating the preferred order that the task should be completed.
GroupUser-definedSpecifies a group name for managing similar tasks. You can sort tasks based on their group. Click the drop-down arrow to select an existing group.

Categories

You can filter the Task List by preconfigured categories. These categories organize concepts or features into groups. When you apply category filters, you focus information within your Task List.

AttributesValueDescription
Set CategoriesN/AFilter tasks or task steps by a predefined grouping.

Template

Click Set to associate a workflow template to a task.

AttributesValueDescription
TemplateUser-definedClick the ellipsis button to select a template from the Task Template folder. To remove the selection, click the Clear button.

Assignments

Task assignments include routing the task to a location or personnel resource depending on the requirement of the workflow.

AttributesValueDescription
PersonnelUser-definedClick the ellipsis button to select the default person that tasks are routed to. To remove the selection, click the Clear button.
LocationUser-definedClick the ellipsis button to select the default location that tasks are routed to. To remove the selection, click the Clear button.