Task Schedules in eSOP
After you create a task, you can schedule it by designating the event that triggers it. If a task should be performed in response to more than one event, you can create multiple schedules for the task. You can also create a schedule without an associated triggering event, such as when you are configuring a task step for manual launch.
Enabling Schedules
For convenience, you can enable or disable at once all schedules associated with a task. To enable or disable individual schedules, select a schedule, and then go to the Status section.
Attributes | Value | Description |
---|---|---|
Enable All | N/A | Click to activate all schedules associated with the task. |
Disable All | N/A | Click to deactivate all schedules associated with the task. |
Insert More Schedules
You can add more schedules to a task. The number of schedules you can add is predetermined by the template.
Attributes | Value | Description |
---|---|---|
Add Schedule | N/A | Click to add a schedule to a task. |
Delete Schedule | N/A | Click to remove a schedule from a task. |
Schedules Tab - General Information
Attributes | Value | Description |
---|---|---|
Name | User-defined | Specifies a unique name assigned to a task. |
Is Schedule Visible in Start Task Window | N/A | Select this check box to ensure that the selected schedule appear in the list of tasks presented when you click the Start Task button. |
Trigger Event
You can set an event that will activate the schedule for execution.
Property | Value | Description |
---|---|---|
Set | User-defined | Click to select a trigger event. |
Clear | N/A | Click to remove the selected event. |
Status
You can choose whether or not a schedule executes as part of the task at run time.
Attributes | Value | Description |
---|---|---|
Enable | User-defined | Click to enable the schedule so that it executes as part of the task at run time. |
Disable | User-defined | Click to disable the schedule so that it does not execute as part of the task at run time. |