Fixed Templates

With fixed templates, the number of steps in the task cannot be increased from the pre-set amount; however, you can remove steps, add missing steps, and re-order the steps.

Usage Restrictions

The following restrictions apply when using fixed templates:
  • If the number of steps in the task is more than the number of steps in the template, the task is invalid.
  • If the template is changed or edited, and the number of steps is less than the number of subprocesses, new steps are not added automatically. The user must add new steps to make the task compatible with the modified template. However, if you change a template to another template that includes no task steps, steps are added automatically.
Note:
If the steps in the fixed template do not match the corresponding subprocesses in the template workflow (that is, they have been moved, added, or deleted), the task steps in the Task Editor are highlighted in yellow. If the linked steps no longer exist in the corresponding template workflow, the task steps are highlighted in red.