Work Data Class Properties Tab

The Properties tab allows you to add, modify, and delete properties that are specific to the selected work data class.

Important:
All relevant production resources, work process segments, work data classes with properties, and work requests must exist in order for a value from one workflow to be recorded in another workflow.

The following table decribes the attributes specific to this resource type.

AttributeValueDescription
ListUser-definedDisplays a list of properties for the selected resource that can be arranged by name, type, and so on, depending on the property. These properties can be inherited from another resource or created for the current resource.
Add PropertyN/AClick to add a new property.
Delete PropertyN/AClick to delete the selected property.
NameUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 50 charactersSpecifies a display name for the selected property.
DescriptionUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 charactersProvides more information about a property that a user may find helpful.
Data TypeSystem-defined Specifies the data type of the property.
Note:
This property cannot be changed if it is inherited from another resource.
ValueUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 8000 charactersSpecifies the value for the selected data type. Valid values depend on the selected data type.
Unit of MeasureUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 20 charactersSpecifies the unit of measure for the data type, such as gallons, inches, tons.