Material Definition Properties
The Properties tab allows you to add, modify, and delete properties that are specific to the selected material definition, and to view the properties for any associated material classes.
The following table describes a property specific to material definitions:
Property | Value | Description |
---|---|---|
Template for Material Lot Property | N/A | Select this check box to make this property available in a material lot. |
The following table describes the information available on the Properties tab, where you can configure the values for the property attributes.
Attribute | Value | Description |
---|---|---|
List | User-defined | Displays a list of properties for the selected resource that can be arranged by name, type, and so on, depending on the property. These properties can be inherited from another resource or created for the current resource. |
Add Property | N/A | Click to add a new property. |
Delete Property | N/A | Click to remove the selected property. |
Name | User-defined alphanumeric string (A–Z, a–z, 0–9) up to 50 characters | Specifies a display name for the selected property. |
Description | User-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 characters | Provides more information about a property that a user may find helpful. |
Type | System-defined | Specifies the data types of the property. Note:
|
Value | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 8000 characters | Specifies the value for the selected data type. The options available depend on the selected data type. |
UoM (Unit of Measure) | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies the unit of measure for the data type, such as gallons, inches, tons. |