Add a material class to a material definition

Before you begin

Note:
You must have added at least one material class resource. For more information, see Add a resource to the material model.

Procedure

  1. In the navigator, click Material.
  2. In the Folders list, select the resource type you want to work with.
    Tip:
    As more lists appear, select the appropriate resource until you find the one you want to work with.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. Click the Classes tab.
  5. Click Add Class.
    The Universal Browser appears.
  6. Select the material class you want to add, and then click OK.
    Tip:
    To remove a material class, from the classes list, select a class, and then click Delete Selection.
  7. Click Save.