Material Classes Properties

The Properties tab allows you to add, modify, and delete properties that are specific to the selected material class.

The following table describes the information available on the Properties tab, where you can configure the values for the property attributes.

AttributeValueDescription
ListUser-definedDisplays a list of properties for the selected resource that can be arranged by name, type, and so on, depending on the property. These properties can be inherited from another resource or created for the current resource.
Add PropertyN/AClick to add a new property.
Delete PropertyN/AClick to remove the selected property.
NameUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 50 charactersSpecifies a display name for the selected property.
DescriptionUser-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 charactersProvides more information about a property that a user may find helpful.
TypeSystem-definedSpecifies the data type of the property.
Note:
  • This property cannot be changed if it is inherited from another resource.
  • When you select Browse for class, the Universal Browser appears where you can select an equipment class.
  • This field is not available if the Linked check box is selected.
ValueUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 8000 charactersSpecifies the value for the selected data type. The options available depend on the selected data type.
UoM (Unit of Measure)User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersSpecifies the unit of measure for the data type, such as gallons, inches, tons.